AXIS#.VL.LIMITP
Description
AXIS#.VL.LIMITP sets the velocity command positive limit.
If the input to the velocity loop is higher than AXIS#.VL.LIMITP, then the actual velocity command AXIS#.VL.CMD is limited by the value of AXIS#.VL.LIMITP.
-
-
ECCN 3A255 imposes special limitations on operating speed for induction motors. See ECCN 3A225 Limitations for Induction Motors.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: RPM See Velocity Units for details. |
|
Range |
Depends on units. See Velocity Range for details. |
|
Default Value |
15000 RPM Depends on units. See Velocity Units for details. |
|
Data Type |
Float |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.VL.LIMITP | 0x5011 | 0x6 | UDINT | - | Velocity | RW | False |
| AXIS2.VL.LIMITP | 0x5111 | 0x6 | UDINT | - | Velocity | RW | False |