AXIS#.WS.STATE
Description
WS switches different current vectors and records position feedback in order to establish commutation alignment.
AXIS#.WS.STATE 0 = wake and shake successful (DONE).
AXIS#.WS.STATE 1 = wake and shake configured and will be done at next enable (ARMED).
AXIS#.WS.STATE 2 = wake and shake running. (ACTIVE)
AXIS#.WS.STATE 10 = error occurred during wake and shake (ERROR).
AXIS#.WS.STATE 11 = wake and shake not required (IDLE).
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
N/A |
Range |
N/A |
Default Value |
Only valid before the first enable occurs. 11 - for feedback types that do not require wake and shake 1 - for feedback types that require wake and shake |
Data Type |
Integer |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus![]() |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT![]() |
AXIS1.WS.STATE | 0x5013 | 0x3 | USINT | - | - | RO | False |
AXIS2.WS.STATE | 0x5113 | 0x3 | USINT | - | - | RO | False |