AXIS#.FAULTS
Description
Indicates what faults are present on an axis.
Examples
In a scenario where two faults are present on Axis 1 (faults 4312 and 4115), the following output would be seen:
-->AXIS1.FAULTS
4312: Feedback: Broken Wire fault.
4115: Failed to set feedback type.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | N/A |
| Range | N/A |
| Default Value | N/A |
| Data Type | String |
| See Also | DRV.FAULTS |
|
Stored in Non Volatile Memory |
No |
Variants Supported
Supported on all device types.