AXIS#.NAME
Description
This parameter is used to set the name of the axis.
Code
-->AXIS1.NAME Axis 1 -->AXIS2.NAME Axis 2 -->AXIS1.NAME Axis 1 -->AXIS2.NAME Axis 2
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
Axis1 for AXIS1 and Axis 2 for AXIS2 |
|
Data Type |
String |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.