DIO#.DIR
Description
Sets or whether the bi-directional IO is an input or output.
| Value | Description |
|---|---|
| 0 | The bi-directional IO is treated as an input signal |
| 1 | The bi-directional IO is treated as an output signal |
Examples
Context
For more information see Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 1 |
| Default Value | 0 (input) |
| Data Type | Integer |
| See Also | |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
DIO1.DIR | 0x368A | 0x1 | USINT | - | - | RW | False |
| DIO2.DIR | 0x368B | 0x1 | USINT | - | - | RW | False | |
| DIO3.DIR | 0x368C | 0x1 | USINT | - | - | RW | False | |
| DIO4.DIR | 0x368D | 0x1 | USINT | - | - | RW | False | |
| DIO5.DIR | 0x368E | 0x1 | USINT | - | - | RW | False | |
| DIO6.DIR | 0x368F | 0x1 | USINT | - | - | RW | False |