DOUT#.SOURCEID

Description

Gets or sets the digital output source id. Value sets the compare engine being used when DOUT#.SOURCE = 3 (Compare)

Examples

Usage

When DOUT#.SOURCE = 3 (Compare) and DOUT#.SOURCEID = 1. DOUT#.STATE will be the result of compare engine 1.

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range N/A
Default Value 0
Data Type Integer
See Also  

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen 0x360A DOUT1.SOURCE 0x1 USINT - - RW False
DOUT2.SOURCE 0x1 USINT - - RW False
DOUT3.SOURCE 0x1 USINT - - RW False
DOUT4.SOURCE 0x1 USINT - - RW False
DOUT5.SOURCE 0x1 USINT - - RW False
DOUT6.SOURCE 0x1 USINT - - RW False
DOUT7.SOURCE 0x1 USINT - - RW False
DOUT8.SOURCE 0x1 USINT - - RW False
DOUT9.SOURCE 0x1 USINT - - RW False