DRV.NAME
Description
This parameter is used to set the name of the drive. The assigned name is one way to identify the drive on a network such as a TCP/IP network on which multiple drives reside. The name is restricted as follows:
- Only use ASCII characters
- Max length of 10 characters
- No spaces in name
Examples
Usage
Issuing DRV.NAME from the terminal with no value will return the name of the drive.
Code
-->DRV.NAME My_AKD2G
-->DRV.NAME
My_AKD2G
-->
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
no_name |
|
Data Type |
String |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.