DRV.REBOOT

Description

This parameter performs a software reboot when the following command is issued in the WorkBench terminal:

DRV.REBOOT 0xAABBCCDD

WorkBench will disconnect from the AKD2G when the reboot command is executed. The AKD2G can be reconnected to WorkBench approximately one minute after the reboot command is issued. The parameters stored in non-volatile memory will be restored to the AKD2G once rebooted.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

Integer

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported