FB#.ENCLINES

Description

Used to configure the number of lines per revolution for rotary encoders. This keyword is only valid for Incremental and Sin/Cos encoders and will be ignored for any other encoders and linear motors.

Examples

Context

See Feedback Devices.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Lines/Rev

Range

0 to 4,294,967,288

Default Value

1024

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen FB1.ENCLINES 0x3500 0x2 UDINT - - RW False
FB2.ENCLINES 0x3501 0x2 UDINT - - RW False
FB3.ENCLINES 0x3502 0x2 UDINT - - RW False
FB4.ENCLINES 0x3503 0x2 UDINT - - RW False
FB5.ENCLINES 0x3504 0x2 UDINT - - RW False