FB#.RESKTR
Description
This parameter sets the resolver nominal transformation ratio. It affects the resolver excitation output amplitude.
The value can be obtained from the resolver data sheet.
Context
See Feedback Devices.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0.001 to 50.000 |
Default Value |
0.5 |
Data Type |
Float |
See Also |
N/A |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
---|---|---|---|---|---|---|---|---|
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | FB1.RESKTR | 0x3500 | 0x4 | UDINT | - | - | RW | False |
FB2.RESKTR | 0x3501 | 0x4 | UDINT | - | - | RW | False | |
FB3.RESKTR | 0x3502 | 0x4 | UDINT | - | - | RW | False | |
FB4.RESKTR | 0x3503 | 0x4 | UDINT | - | - | RW | False | |
FB5.RESKTR | 0x3504 | 0x4 | UDINT | - | - | RW | False |