REC.TRIGVAL
Description
REC.TRIGVAL is the value that must be met by REC.TRIGPARAM for the trigger to occur. The units of this parameter are set according to the units of REC.TRIGPARAM.
Examples
Code
Sets the value to use as trigger to be 1024. Only when REC.TRIGPARAM matches this value determined by what REC.TRIGTYPE is set to, will the triggering happen.
-->REC.TRIGVAL 1024
Context
For more information see Scope.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
The units of the parameter are chosen according to the unit type. |
|
Range |
-9223372036854775.808 to 9223372036854775.807 |
|
Default Value |
0 |
|
Data Type |
Float |
|
See Also |
|
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.