BODE.IFLIMIT
Description
When BODE.MODE is set to 5, the firmware monitors the drive current (IL.CMD ). When IL.CMD goes above BODE.IFTHRESH, an internal counter records the length of time IL.CMD was above BODE.IFTHRESH. If the internal counter reaches BODE.IFLIMIT, Fault 133 – Instability during Autotune will be generated.
The smaller BODE.IFLIMIT, the quicker Fault 133 will be generated when IL.CMD exceeds BODE.IFLIMIT.
Example
Set BODE.IFTHRESH to 6 Amps:
-->BODE.IFTHRESH 6
Set BODE.IFLIMIT to 0.500 seconds:
-->BODE.IFLIMIT 0.5
Set BODE.MODE to 5 to enable stability detection:
BODE.MODE 5
General Information
|
Type |
R/W Parameter |
|
Units |
s |
|
Range |
0.001 to 60.000 |
|
Default Value |
0 |
|
Data Type |
Decimal |
|
Start Version |
M_01-02-10-000 |
Related Topics
Using the Performance Servo Tuner
Using the Performance Servo Tuner: Advanced
BODE.MODE,BODE.MODETIMER, BODE.IFTHRESH, BODE.VFLIMIT, BODE.VFTHRESH