COGCOMP.V
Description
Velocity for the move during automatic teaching of the cogging compensation table.
General Information
This content is not applicable to KAS.
|
Type |
NV Parameter |
|
Units |
Depends on UNIT.VROTARY or UNIT.VLINEAR Rotary: rpm, rps, deg/s, (custom units)/s, rad/s Linear: counts/s, mm/s, µm/s, (custom units)/s |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
Start Version |
M_01-14-06-001 |
| Fieldbus |
Index/Subindex | Object Start Version |
|---|---|---|
|
5414h/0 |
M_01-14-06-001 |
Related Topics