DRV.FEATURES
Description
DRV.FEATURES returns a list of strings that describes specific features for the this firmware. The list is read only and is dependent on the firmware version. The purpose of this keywords is to activate certain views and behavior in workbench that are useful for these specific features.
Example
-->DRV.FEATURES
001: Spaces in strings
002: WS.MODE 2 Available
003: Telnet Message Grouping
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | M_01-00-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
"" |
|
Data Type |
String |
|
Stored in Non Volatile Memory |
No |
This keyword is not accessible via fieldbus.