DRV.LOGICVOLTS
Description
DRV.LOGICVOLTS reads the logic voltages data of 1.2 V, 2.5 V, 3.3 V, 5 V, 12 V, –12 V, and 3.3 AV.
Example
Below is an example of the output for this command:
ch0 = 1.2V : 1211 mv
ch1 = 2.5V :2488 mv
ch2 = 3.3V :3274 mv
ch3 = 5V :4950 mv
ch4 = 12V :11892 mv
ch5 = -12V :-11912 mv
ch6 = 3.3AV :3300 mv
ch7 = R ohm :100000 ohm
General Information
|
Type |
R/O Parameter |
|
Units |
mv , Ω |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
Start Version |
M_01-00-00-000 |