DRV.REBOOT
Description
This parameter performs a software reboot when the following command is issued in the WorkBench terminal:
DRV.REBOOT 0xAABBCCDD
WorkBench will disconnect from the AKD when the reboot command is executed. The AKD can be reconnected to WorkBench approximately one minute after the reboot command is issued. The parameters stored in non-volatile memory will be restored to the AKD once rebooted.
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
Start Version |
M_01-13-08-000 |