ECAT.LEGACYREV
Description
The ECAT.LEGACYREV defines the revision number located in the EtherCAT
EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs slave information (EEprom).
| Value | Description |
|---|---|
| 0 | Revision number is set to actual revision (e.g. for FW 1.16 #x00160000). Note: The revision number will change with for next releases. |
| 1 | Revision number is set to legacy value of #x00000002. |
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
0 to 1 |
|
Default Value |
1 |
|
Data Type |
Integer |
|
Start Version |
M_01-16-00-001 |
| Fieldbus |
Index/Subindex | Object Start Version |
|---|---|---|
|
EtherCAT COE and CANopen |
541Dh/1 | M_01-16-00-001 |