FBUS.STATE
Description
FBUS.STATE returns the current state of the fieldbus. The value returned is dependent upon the fieldbus being used.
| Value | CANopen over CAN |
CANopen over EtherCAT |
|---|---|---|
| -1 | Not connected | Not connected |
| 0 | Init. | - |
| 1 | N/A | Init. |
| 2 | N/A | Pre-operational |
| 3 | - | Boot |
| 4 | Stopped | Safe-operational |
| 5 | Operational | - |
| 8 | - | Operational |
| 127 | Pre-operational | - |
General Information
|
Type |
R/O |
|
Units |
N/A |
|
Range |
Depends on fieldbus. See table below. |
|
Default Value |
Depends on fieldbus. See table below. |
|
Data Type |
Integer |
|
Start Version |
M_01-08-00-000 |