IL.IVFB
Description
IL
"Instruction list"
This is a low-level language and resembles assembly.IVFB is an offset value that is added to the measured current in the u-winding of the motor. This value is used for compensating for an error in the current measurement. The drive measures 256 times the current in the u-winding when powering-up the drive. Afterwards, the drive calculates the average value of the measured current and uses this value for the offset value.
General Information
|
Type |
R/O Parameter |
|
Units |
A |
|
Range |
± Drive peak current (DRV.IPEAK) |
|
Default Value |
0 A |
|
Data Type |
Float |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |
Related Topics
1 Current Loop