IL.PWMFREQ
Description
IL
"Instruction list"
This is a low-level language and resembles assembly.PWMFREQ reads the PWM frequency of the IGBTs.
General Information
|
Type |
R/O Parameter |
|
Units |
kHz |
|
Range |
0 to 200 kHz |
|
Default Value |
8 kHz |
|
Data Type |
Float |
|
See Also |
N/A |
|
Start Version |
M_01-00-00-000 |