REC.CH1 to REC.CH6
Description
REC.CHx specifies the recording channels.
There are 3 options to set the recording channels values:
- Set 0, CLR, or CLEAR. This setting clears the recording channel.
- Set one of the recordable commands. The list of recordable commands can be obtain by executing REC.RECPRMLIST.
- Set an internal value or variable of the drive (same as for DRV.MEMADDR input).
General Information
|
Type |
R/W Parameter |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
CH1 = IL CH2 = IL.CMD CH3 = VL.FB CH4 = Empty CH5 = Empty CH6 = Empty |
|
Default Value |
CH1 = STRINGS.I2TVALUE CH2 = STRINGS.IVALUE CH3 = STRINGS.STOSTATE |
|
Data Type |
String |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
Related Topics