REC.OFF
Description
REC.OFF turns the recorder off. In order to set the recorder again, the recorder must first be armed and then a trigger set.
General Information
|
Type |
R/W Parameter |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
REC.ACTIVE, REC.DONE |
|
Start Version |
M_01-00-00-000 |
*For Profinet, write a value of 0 into the PNU to execute a command.
Related Topics
REC.READY