REC.RETRIEVESIZE
Description
This parameter sets the number of samples that REC.RETRIEVEDATA returns.
WorkBench also uses this parameter to set the number of samples returned when retrieving the data continuously for RT recoding.
Use REC.RETRIEVE for the complete recording information view.
General Information
|
Type |
R/W Parameter |
|
Units |
recorder samples |
|
Range |
0 to 65,535 recorder samples |
|
Default Value |
1,000 recorder samples |
|
Data Type |
Integer |
|
See Also |
|
|
Start Version |
M_01-00-00-000 |
Related Topics