REC.TRIGMASK
Description
The keyword REC.TRIGMASK is only active when the trigger type (REC.TRIGTYPE) for the recorder is set to 5, which means "Bit Mask Parameter". The trigger is executed once the trigger level (REC.TRGIVAL) matches the data of the trigger parameter (REG.TRIGPARAM) bitwise mask with REC.TIRGMASK.
General Information
|
Type |
Read / Write |
|
Units |
N/A |
|
Range |
0 to 2^63-1 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
REC.TRIG |
|
Start Version |
M_01-00-00-000 |