REC.TRIGPRMLIST
Description
This command returns the list of trigger parameters. Each one of those parameters can serve as the trigger parameter (input to REC.TRIGPARAM).
Note that an internal address or a registered variable can be used as input to REC.TRIGPARAM in addition to the list that this parameter returns.
General Information
|
Type |
R/O Parameter |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
REC.TRIGPARAM |
|
Start Version |
M_01-00-00-000 |
Related Topics