REC.TRIGTYPE
Description
REC.TRIGTYPE sets the type of trigger.
Input values are as follows:
|
Value |
Description |
|---|---|
|
0 |
Recording starts immediately |
|
1 |
Recording starts on the next command executed through the TCP/IP. The trigger location in the buffer is set according to REC.TRIGPOS. |
|
2 |
Recording starts per the values of REC.TRIGPARAM, REC.TRIGVAL, REC.TRIGSLOPE, and REC.TRIGPOS. |
|
3 |
Recording starts when the value of REC.TRIGPARAM is 0 for REC.TRIGSLOPE = 0 or 1 for REC.TRIGSLOPE = 1 |
General Information
|
Type |
R/W Parameter |
|
Units |
0 = immediate 1 = command 2 = parameter 3 = boolean |
|
Range |
0 to 3 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
REC.TRIG , REC.TRIGPARAM, REC.TRIGVAL, REC.TRIGSLOPE REC.TRIGPOS |
|
Start Version |
M_01-00-00-000 |
Related Topics