REC.TRIGVAL
Description
REC.TRIGVAL is the value that must be met by REC.TRIGPARAM for the trigger to occur. The units of this parameter are set according to the units of REC.TRIGPARAM.
General Information
|
Type |
R/W Parameter |
|
Units |
The units of the parameter are chosen according to the unit type. |
|
Range |
-9223372036854775.808 to 9223372036854775.807 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
See Also |
REC.TRIG , REC.TRIGPARAM, REC.TRIGVAL, REC.TRIGSLOPE, REC.TRIGPOS |
|
Start Version |
M_01-00-00-000 |
Related Topics