ANY_TO_LINT / ANY_TO_ULINT
Inputs
IN : ANY Input value
Outputs
Q : LINT Value converted to long (64 bit) integer
Remarks
For BOOL input data types, the output is 0 or 1. For REAL input data type, the output
is the integer part of the input real. For TIME input data types, the result is the number
of milliseconds. For STRING inputs, the output is the number represented by the string, or
0 if the string does not represent a valid number. In FFLD language, the conversion is
executed only if the input rung (EN) is TRUE. The output rung (ENO) keeps the same value
as the input rung. In IL
"Instruction list"
This is a low-level language and resembles assembly Language, the ANY_TO_LINT function converts the current result.
ST Language
Q := ANY_TO_LINT (IN);
FBD Language
FFLD Language
(* The conversion is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)
IL Language:
Op1: FFLD IN
ANY_TO_LINT
ST Q
See also
ANY_TO_BOOL ANY_TO_SINT ANY_TO_INT ANY_TO_DINT ANY_TO_REAL ANY_TO_LREAL ANY_TO_TIME ANY_TO_STRING