Bookmarks
Below are the available commands for using bookmarks:
|
Ctrl + F2 |
Toggle the bookmark at the current position |
|
Shift + F2 |
Go to the next bookmark |
According to the type of document, the possible locations for a bookmark are:
- In the text editor, a bookmark is placed on a line of
text.
- In the SFC
"Sequential function chart"
It can be used to program processes that can be split into steps.
The main components of SFC are:
- Steps with associated actions
- Transitions with associated logic conditions
- Directed links between steps and transitions editor, a bookmark is placed on an SFC symbol (step, transition,
jump...).
- In the FBD
"Function block diagram"
A function block diagram describes a function between input variables and output variables. A function is described as a set of elementary blocks editor, a bookmark is placed on any FBD object (not on a line).
- In the FFLD editor, a bookmark is placed on a rung header.
- In the Variable editor, a bookmark is placed on any line of the grid (variable
or group).
-
-
Bookmarks are valid only while the editing window is open; they are not stored in the document when the window is closed.