Boolean operations
| AND | performs a Boolean AND |
| OR | performs a Boolean OR |
| XOR | performs an exclusive OR |
| NOT | performs a Boolean negation of its input |
| QOR | qualified OR |
| S | force a Boolean output to TRUE |
| R | force a Boolean output to FALSE |
Below are the available blocks for managing Boolean signals:
| RS | reset dominant bistable |
| SR | set dominant bistable |
| R_TRIG | rising pulse detection |
| F_TRIG | falling pulse detection |
| SEMA | semaphore |
| FLIPFLOP | flipflop^bistable |