ON
The ON instruction provides a simpler syntax for checking the rising edge
A rising edge is the transition of a digital signal from low to high. It is also called positive edge of a Boolean condition.
Syntax
ON <BOOL expression> DO
<statements>
END_DO;
Remarks
Statements within the ON structure are executed only when the Boolean expression rises from FALSE to TRUE. The ON instruction avoids systematic use of the R_TRIG function block or other "last state" flags.
The ON syntax is available in any program, sub-program or UDFB
"User Defined Function Block"
UDFB can be used as a sub-function block in another program of the application. It is described using FBD, LD, ST or IL language. Input / output parameters of a UDFB (as well as private variables) are declared in the variable editor as local variables of the UDFB.
This statement is an extension to the standard and is not IEC61131-3
IEC 61131-3 is the third part of the open international standard IEC 61131. The current (second) edition was published in 2003.
IEC 61131-3 currently defines five programming languages for programmable control systems
It deals with programming languages and defines two graphical and two textual PLC programming language standards compliant.
-
-
This instruction should not be used inside UDFBs. This instruction is not UDFB safe.
ST Language
(* This example counts the rising edges of variable bIN *) ON bIN DO
diCount := diCount + 1;
END_DO;