Move or copy SFC charts
"Sequential function chart"
It can be used to program processes that can be split into steps.
The main components of SFC are:
- Steps with associated actions
- Transitions with associated logic conditions
- Directed links between steps and transitions Editor fully supports drag-and-drop for moving or copying items. To move an item, select and drag it to the desired position.
To copy an item, do the same, and just press the Ctrl key while dragging. It is also possible to drag pieces of a chart from one program to another if both are open and visible on the screen.
At any moment, while dragging items, you can press ESCAPE to cancel the operation.
Alternatively, you can use the Copy / Cut / Paste commands from the Edit menu. The Paste action is performed at the current position.