Renumber steps and transitions
"Sequential function chart"
It can be used to program processes that can be split into steps.
The main components of SFC are:
- Steps with associated actions
- Transitions with associated logic conditions
- Directed links between steps and transitions Editor allocates a new
number to each step or transition inserted in the chart.
To change the number of a step, transition or jump, select it and press Ctrl+ENTER.
It is not possible to change the number of a step or a transition if its level 2 is currently open for editing. The number is used for identifying the step or transition in the level 2 editing window.
In compiler reports, a step is identified by its number prefixed by "GS". A transition is identified by its number prefixed by "GT".