ST / IL Drag-and-drop features
"Structured text"
A high-level language that is block structured and syntactically resembles Pascal / IL
"Instruction list"
This is a low-level language and resembles assembly Editor supports powerful drag-and-drop features that
help you to develop and test your programs. You can:
- Drag text (words or lines) from the ST / IL editor to another application (such as a text editor)
- Do the opposite
- Drag a variable symbol from the variable editor to the ST / IL editor
- Drag a variable symbol from the ST / IL editor to the watch list (*)
(*) When dragging the symbol of an array to the watch list, all items in the array are added to the watch list.