Brake
The brake output on connector X2 controls a mechanical brake that optionally may be fitted to a motor. The brake is applied and released relative to the Drive Active state of the drive. You can modify the release and apply delays using the parameters shown below.
The brake output on connector X9 controls a mechanical brake that optionally may be fitted to a motor. The brake is applied and released relative to the Drive Active state of the drive. You can modify the release and apply delays using the parameters shown below.
|
Button or Dialog Box |
Description |
Parameter |
|---|---|---|
|
Brake Control |
Sets whether the motor has a brake. |
|
|
Time to Release |
The time, set by the user, required to mechanically disengage the brake. After this time, motion commands are accepted. |
|
|
Time to Apply |
The time, set by the user, required to mechanically engage the brake. After this time, the drive will disable. |