VBUS.DCOPERATION

Description

This parameter indicates whether the mains input is DC or AC.

If the mains input in DC and it is connected to DC+/DC- terminals (X3), not setting this parameter to 1 will cause “AC input phase loss” error.


  • If using DC mains, Kollmorgen recommends that the mains input is connected to RST terminal as opposed to DC+/DC- terminal.
  • The reason is that the voltage of DC+/DC- may go above the mains voltage in regenerative breaking mode, and this can damage the DC power supply feeding the drive.

Examples

Usage

If the parameter is set to 0 ->1, the drive assumes that the mains input is DC, and phase loss detection as well as power loss detection are turned off.

If the parameter is set to 1 ->0, the drive assumes that the mains input is AC, and depending on the status of VBUS.THREEPHASE phase loss detection may be turned on.

Code

--> VBUS.DCOPERATION 0
--> DRV.FAULTS
1-2014: AC input phase loss.
2-2014: AC input phase loss.			
--> VBUS.DCOPERATION 1
--> DRV.FAULTS
No faults active

General Information

Type Read/Write
Units N/A
Range 0 (ac mains) to 1 (dc mains)
Default Type 0 (ac mains)
See Also VBUS.THREEPHASE
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.