MLAxisDriveNumber
Description
This function block returns the drive number that is associated with the axis, or -1 if the function block failed.
Figure 7-80: ML_AxisDriveNumber
-
- MLPNAxisCreate assigns the drive axis number.
Arguments
Input
| AxisID | Description | ID name of the Axis |
| Data type | DINT | |
| Range | — | |
| Unit | N/A | |
| Default | — |
Output
| OK | Description | Returns true when the function successfully executes |
| Data type | BOOL | |
| Range | N/A | |
| Unit | N/A | |
| DriveAxisNumber | Description | Drive number that is associated with the axis, or -1 if the function block failed. |
| Data type | INT | |
| Range | -1 or [1,32767] | |
| Unit | N/A |
Related Functions
___
Example
Structured Text
Inst_MLAxisDriveNumber( AxisID)
IF Inst_MLAxisDriveNumber.OK Then
Axis1DriveNumber := Inst_MLAxisDriveNumber.DriveAxisNumber
End_IF;
Ladder Diagram
Function Block Diagram