MLAxisGenPos
Description
Returns the generator position of the axis Returns TRUE if the internal generator axis is ready.
-
-
This function or function block returns cached data. See Programming a Dual Core Controller for more information.
Arguments
Input
|
ID |
Description |
ID Name of the Axis block |
|
Data type |
DINT |
|
|
Range |
— |
|
|
Unit |
N/A |
|
|
Default |
— |
Output
|
Default (.Q) |
Description |
Returns true when function successfully executes See more details here. |
|
Data type |
BOOL |
|
|
Unit |
N/A |
|
|
Position |
Description |
Returns Axis generator position value |
|
Data type |
LREAL |
|
|
Unit |
Related Functions
Example
Structured Text
|
Axis1_Generator_Position := MLAxisGenPos(PipeNetwork.Axis1 ) ;
|
Ladder Diagram
Function Block Diagram
[Top]