MLAxisReAlign
Description
When stopping the drive a motion profile is applied to decelerate. During the deceleration, the Reference position changes. Calling MLAxisReAlign realigns the actual position with the reference position by moving the axis by the specified delta position, which is typically calculated by the application code. After a MLAxisStop is executed, a MLAxisReAlign is required for the Pipe Position to be used again (see more details about the Restarting Motion here).
The function returns TRUE if it succeeds.
-
-
The realign function do not work properly if the MLAxisStop function is continuously executed via its Start input
Arguments
Input
| ID |
Description |
ID Name of the Axis block. |
|
Data type |
DINT |
|
|
Range |
— |
|
|
Unit |
N/A |
|
|
Default |
— |
|
| Acceleration |
Description |
Sets the Realign Acceleration. |
|
Data type |
LREAL |
|
|
Range |
— |
|
|
Unit |
User unit/sec2 |
|
|
Default |
— |
|
| Deceleration |
Description |
Sets the Realign Deceleration rate. |
|
Data type |
LREAL |
|
|
Range |
— |
|
|
Unit |
User unit/sec2 |
|
|
Default |
— |
|
| Speed |
Description |
Sets the Axis Speed. |
|
Data type |
LREAL |
|
|
Range |
— |
|
|
Unit |
User unit/sec |
|
|
Default |
— |
|
| DeltaPos |
Description |
Sets the Axis Delta Position, or the relative distance to be moved. |
|
Data type |
LREAL |
|
|
Range |
— |
|
|
Unit |
||
|
Default |
— |
Output
|
Default (.Q) |
Description |
Returns true when function successfully executes. See more details here. |
|
Data type |
BOOL |
|
|
Unit |
N/A |
Related Functions
Example
Structured Text
|
MLAxisReAlign(PipeNetwork.Axis1, 100000, 100000, 500, 20 ) ;
|
Ladder Diagram
Function Block Diagram
[Top]