MLAxisReadVel
Description
Return the actual velocity of the axis as calculated internally by the drive mapped to it, based on the data provided by the feedback device
A process whereby some proportion of the output signal of a system is passed (fed back) to the input.
In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position of the drive.
-
-
This function or function block returns cached data. See Programming a Dual Core Controller for more information.
Arguments
Input
|
ID |
Description |
Pipe network identifier of the axis block. |
|
Data type |
DINT |
|
|
Range |
— |
|
|
Unit |
N/A |
|
|
Default |
— |
Output
|
Velocity |
Description |
Actual velocity returned by the drive associated to the axis. |
|
Data type |
LREAL |
|
|
Unit |
User unit/sec |
Related Functions
Example
Structured Text
|
Axis1_Velocity := MLAxisReadVel(PipeNetwork.Axis1 ) ;
|
Ladder Diagram
Function Block Diagram
[Top]