MC_GrpSetOverride

Description
MC_GrpSetOverride sets the velocity factor that is multiplied to the commanded velocity of all axes in the group. This function block in itself does not cause any motion.
Figure 7-172: MC_GrpSetOverride
Related Functions
Coordinated Motion, the top-level topic for Coordinated Motion.
Arguments
For more detail on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules.
Input
| Enable | Description | On the rising edge |
| Data type | BOOL | |
| Range | 0, 1 | |
| Unit | N/A | |
| Default | — | |
| AxesGroup | Description | The axes group in which the velocity multiplier will be applied. |
| Data type | AXES_GROUP_REF | |
| Range | N/A | |
| Unit | N/A | |
| Default | — | |
| VelFactor | Description | The new multiplier factor for the commanded velocity of the axes group. |
| Data type | REAL | |
| Range | [0.0 .. 2.0] | |
| Unit | N/A | |
| Default | — |
Output
| Enabled | Description | Indicates that the override was successful. |
| Data type | BOOL | |
| Busy | Description | If True, then the FB is executing. |
| Data type | BOOL | |
| Error | Description | If True, an error has occurred. |
| Data type | BOOL | |
| ErrorID | Description | Indicates the error identifier if Error output is set to TRUE. See the table PLCopen Function Block ErrorID Output. |
| Data type | INT |
Example
ST
Inst_MC_GrpSetOverride( EnableOverride, Group1_Ref, VelocityFactor );
IL
BEGIN_IL
"Instruction list"
This is a low-level language and resembles assembly
CAL Inst_MC_GrpSetOverride( EnableOverride, Group1_Ref, VelocityFactor )
END_IL
FBD
FFLD
[Top]