MC_GrpReadBoolPar

Description
This function block reads a value from the specified Boolean group parameter. See Recovery of the System State After an Axis Error for more information.
MC_GrpReadBoolPar( Axesgroup_Ref GroupID, Uint BoolID) where BoolID can be one of the following 2 currently defined Booleans:
IGNORE_AXIS_ESTOP: ID = 1000 : The value read will be either TRUE or False as set by the MC_GrpWriteBoolPar function block.
AXIS_ESTOP_ACTIVE: ID = 1001 : This Read-only parameter will be asserted TRUE whenever an axis in the group is experiencing an Axis Estop Error. When there are no Axis Estop Errors present on the axes in a group, this parameter will be set to FALSE.
Figure 7-155: MC_GrpReadBoolPar
-
-
This function or function block returns cached data. See Programming a Dual Core Controller for more information.
Related Function Blocks
MC_GrpWriteBoolPar,MC_ErrorDescription
Coordinated Motion, the top-level topic for Coordinated Motion.
Arguments
For more details on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules.
Input
| Enable | Description | If True, then request to read a value from the specified Boolean group parameter. |
| Data Type | BOOL | |
| Range | 0, 1 | |
| Unit | N/A | |
| Default | — | |
| AxesGroupRef | Description | The axis group that the Boolean parameter value will be read from. |
| Data Type | AXES_GROUP_REF | |
| Range | N/A | |
| Unit | N/A | |
| Default | — | |
| ParamNum | Description |
ParamNum can be one of the following two currently defined Booleans:
|
| Data Type | UINT | |
| Range | 1000, 1001 | |
| Unit | UINT | |
| Default | — |
Output
| Done | Description |
If True, then the command completed successfully. |
| Data Type | BOOL | |
| Error | Description |
If True, an error has occurred. |
| Data Type | BOOL | |
| ErrorID | Description | Indicates the error if Error output is set to TRUE. See the table in PLCopen Function Block ErrorID Output. |
| Data Type | INT | |
| ParamValue | Description | True or False |
| Data Type | BOOL |
Example
ST
Inst_GrpReadBoolPar( DoEnable, Group1_Ref, AXIS_ESTOP_ACTIVE );
IL
BEGIN_IL
"Instruction list"
This is a low-level language and resembles assembly
Cal Inst_GrpReadBoolPar( DoEnable, Group1_Ref, AXIS_ESTOP_ACTIVE )
END_IL
FBD
FFLD
[Top]