FileDelete
Description
This function block removes a file from the file system.
Figure 7-194: The FileDelete Function Block
Related Functions
FileCopy, FileRename, FileExists, FileSize
See also: File Management
Arguments
Input
| Execute | Description | On the rising edge |
| Data Type | BOOL | |
| Range | 0, 1 | |
| Unit | N/A | |
| Default | — | |
| Path | Description | The path to the file to be deleted |
| Data Type | STRING | |
| Range | N/A | |
| Unit | N/A | |
| Default | — |
Output
| Done | Description | If TRUE, then the command completed successfully |
| Data Type | BOOL | |
| Error | Description | If TRUE, an error has occurred |
| Data Type | BOOL | |
| ErrorID | Description | Indicates the error if Error output is set to TRUE. See the table in Search IndexFile and TCP/IP Function Block ErrorID Output |
| Data Type | DINT |
Example
Structured Text
(* FileDelete example *)
CASE StepCounter OF
0:
Inst_FileDelete(TRUE, 'Test.txt');
StepCounter := StepCounter + 1;
1:
Inst_FileDelete(TRUE, 'Test.txt');
IF Inst_FileDelete.Done THEN
Inst_FileDelete(FALSE, '');
StepCounter := StepCounter + 1;
END_IF;
END_CASE;