FileWriteBinData
Description
This function block writes binary data to a file. Before using FileWriteBinData, you may use SerializeOut to copy variable data to a binary frame.
Figure 7-205: The FileWriteLine Function Block
Related Functions
FileClose, FileEOF, FileOpenA, FileOpenR, FileOpenW, FileReadBinData, FileReadLine, FileSeek, FileWriteLine
See also: File Management
Arguments
Input
| Execute | Description | On the rising edge |
| Data Type | BOOL | |
| Range | 0, 1 | |
| Unit | N/A | |
| Default | — | |
| ID | Description | ID of the open file. |
| Data Type | UDINT | |
| Range | N/A | |
| Unit | N/A | |
| Default | — | |
| Frame |
Description | The array of binary data to write |
| Data Type | USINT[] | |
| Range | N/A | |
| Unit | N/A | |
| Default | — | |
| FrameSize | Description | Number of bytes to write from the Frame array. |
| Data Type | DINT | |
| Range | N/A | |
| Unit | N/A | |
| Default | — |
Output
| Done | Description | If TRUE, then the command completed successfully |
| Data Type | BOOL | |
| Error | Description | If TRUE, an error has occurred |
| Data Type | BOOL | |
| ErrorID | Description | Indicates the error if Error output is set to TRUE. See the table in Search IndexFile and TCP/IP Function Block ErrorID Output |
| Data Type | DINT |
Example
Structured Text
(* FileWriteBinData example *)
CASE StepCounter OF
0:
Inst_FileWriteBinData(TRUE, MyOutputFileID, OutputFrame, 128);
StepCounter := StepCounter + 1;
1:
Inst_FileWriteBinData(TRUE, MyOutputFileID, OutputFrame, 128);
IF Inst_FileWriteBinData.Done THEN
Inst_FileWriteBinData(FALSE, 0, OutputFrame, 0);
StepCounter := StepCounter + 1;
END_IF;
END_CASE;