GetCtrlInfo

This function block returns a String containing the value of the control parameter requested.
Arguments
Input
| Execute | Description | Rising edge of enable initiates read of parameter | |||||||||||||||||||||
| Data Type | BOOL | ||||||||||||||||||||||
| Range | 0, 1 | ||||||||||||||||||||||
| Unit | N/A | ||||||||||||||||||||||
| Default | — | ||||||||||||||||||||||
| Parameter Number | Description | Parameter number to read | |||||||||||||||||||||
| Data Type | INT | ||||||||||||||||||||||
| Range | [1,6] | ||||||||||||||||||||||
| Unit | N/A | ||||||||||||||||||||||
| Value Description |
These parameters are also Internal Defines, as shown in the table below.
|
Output
| Done | Description | Indication that read completed without error | |||||||||||||||
| Data Type | BOOL | ||||||||||||||||
| Error | Description | Indication that read completed with error | |||||||||||||||
| Data Type | BOOL | ||||||||||||||||
| ErrorID | Description | Error value to indicate error condition | |||||||||||||||
| Data Type |
INT These parameters are also Internal Defines, as shown in the table below.
|
||||||||||||||||
| Value | Description | String containing data that was read. | |||||||||||||||
| Data Type | STRING |
Examples
Structured Text
Inst_GetCtrlInfo( ExecuteRead, CTRLINFO_SERIAL_NUMBER); if Inst_GetCtrlInfo.Done then serialNumber := Inst_GetCtrlInfo.Value; end_if;
Ladder Diagram
[Top]