MC_ReadActVel
Description
-
-
This function or function block returns cached data. See Programming a Dual Core Controller for more information.
Arguments
For more detail on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules
Input
| Enable | Description | Requests to read the axis's actual velocity |
| Data type | BOOL | |
| Range | 0, 1 | |
| Unit | N/A | |
| Default | — | |
| Axis | Description | Name of a declared instance of the AXIS_REF library function. For more details, About Axis Name and Number |
| Data type | AXIS_REF | |
| Range | [1,256] | |
| Unit | N/A | |
| Default | — |
Output
| Valid | Description | Indicates the value at the ActualVelocity output is available |
| Data type | BOOL | |
| Busy | Description | Indicates this function block is executing |
| Data type | BOOL | |
| Error | Description | Indicates an invalid input |
| Data type | BOOL | |
| ErrorID | Description | Indicates the error if Error output is set to TRUE. |
| Data type | INT | |
| ActualVelocity | Description |
Actual velocity of the axis. Please note that oscillations may be seen due to this being an instant velocity, not an average velocity. |
| Unit | User unit/sec | |
| Data type | LREAL |
Example
Structured Text
* MC_ReadActVel S
T example *);
Inst_MC_ReadActVel( TRUE, Axis1 ); //Inst_MC_ReadActVel is an instance of MC_ReadActVel function block
ActualVel := Inst_MC_ReadActVel.ActualVelocity; // store ActualVelocity output into a user defined variable
Ladder Diagram
[Top]