MC_ReadAxisErr
Description
A function block groups an algorithm and a set of private data. It has inputs and outputs. MC_ReadAxisErr returns the error status of the specified axis.
-
-
This function or function block returns cached data. See Programming a Dual Core Controller for more information.
Arguments
For more detail on how inputs and outputs work, refer to PLCopen Function Blocks - General Rules
Input
|
Enable |
Description |
requests to read the error status of the axis |
|
Data type |
BOOL |
|
|
Range |
0, 1 |
|
|
Unit |
N/A |
|
|
Default |
— |
|
|
Axis |
Description |
Name of a declared instance of the AXIS_REF library function. For more details,About Axis Name and Number |
|
Data type |
||
|
Range |
[1,256] |
|
|
Unit |
N/A |
|
|
Default |
— |
Output
|
Valid |
Description |
Indicates the AxisErrorID output is valid |
|
Data type |
BOOL |
|
|
Busy |
Description |
Indicates this function block is executing |
|
Data type |
BOOL |
|
|
Error |
Description |
Indicates an invalid input |
|
Data type |
BOOL |
|
|
ErrorID |
Description |
Indicates the error if Error output is set to TRUE
|
|
Data type |
INT |
|
|
AxisErrorID |
Description |
Indicates the error status of the axis. Each bit indicates a specific error. Both emergency-stop (E-stop) and controlled-stop (C-stop) errors are indicated. The table below defines the bits of this output. |
|
Data type |
INT |
| Hexadecimal | Decimal | Description |
|---|---|---|
| 0000H | 0 | No Error |
| 0001H | 1 | User-set E-stop via MC_EStop, E-stop |
| 0002H | 2 | Loss of Feedback, E-stop |
| 0004H | 4 | Drive Fault, E-stop |
| 0008H | 8 | Drive Communication Failure, E-stop |
| 0400H | 1024 | Synchronization Error, C-stop |
| 0700H | 7192 | Drive Overtravel Limit Exceeded, Cstop (see Overtravel Conditions) |
-
-
Multiple errors can be active at the same time. For example, if a User-set E-stop and an Excess Position Error E-stop are both active, the value would be 00000011H (17 decimal).
Example
Structured Text
(* MC_ReadAxisErr ST example *)
Inst_MC_ReadAxisErr( TRUE, Axis1 );
//Inst_MC_ReadAxisErr is an instance of MC_ReadAxisErr function block
AxisErrorBits := Inst_MC_ReadAxisErr.AxisErrorID; //AxisErrorID contains the error bits
Ladder Diagram
[Top]