MLFB_HomeFindLimitInput
Description
The find limit input mode moves to a limit input. This method can be used if you have a positive or negative limit switch available that you want to establish as a home reference point.
Arguments
Input
|
ibExecute |
Description |
Start homing, edge-triggered |
|
Data type |
BOOL |
|
|
iAxisID |
Description |
ID of Axis block of Pipe Network |
|
Data type |
DINT |
|
|
iPosition |
Description |
Reference position |
|
Data type |
LREAL |
|
|
ibDirection |
Description |
0=positive, 1=negative |
|
Data type |
BOOL |
|
|
iVelocity |
Description |
Reference speed |
|
Data type |
LREAL |
|
|
iAcceleration |
Description |
Reference acceleration |
|
Data type |
LREAL |
|
|
iDeceleration |
Description |
Reference deceleration |
|
Data type |
LREAL |
|
|
ibLimitSwitch |
Description |
Pos. or neg. limit switch, high-active (depends on ibDirection) |
|
Data type |
BOOL |
|
|
iTimeout |
Description |
Time monitoring (T#0ms: off) |
|
Data type |
TIME |
Output
|
obDone |
Description |
Done bit |
||||||||||||
|
Data type |
BOOL |
|||||||||||||
|
obActive |
Description |
Active bit |
||||||||||||
|
Data type |
BOOL |
|||||||||||||
|
obError |
Description |
Error bit |
||||||||||||
|
Data type |
BOOL |
|||||||||||||
|
oErrorID |
Description |
Error identifier, see list here
|
||||||||||||
|
Data type |
DINT |
Example
ST
//Call homing function on Axis1 with preset velocity, accel, and decel values
//Start in negative direction and stop when axis hits limit switch or times out
//after seeing limit switch, set axis position to zero
Inst_MLFB_HomeFindLimitInput( StartHomeRoutine,
PipeNetwork.AXIS1,
0,
TRUE,
100,
1000,
1000,
HomeDigitalInput,
T#30s );
HomeDone := Inst_MLFB_HomeFindLimitInput.obDone;
Function Block Diagram
FFLD
[Top]