MLMotionStop

Description
Stops the motion bus driver, motion engine, and EtherCAT
EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs network operation, resulting in the EtherCAT network transitioning to the Init state. Returns TRUE if the function succeeded.
See also: MLMotionStart, MLMotionRstErr, MLMotionStatus
Return Type
BOOL
Example
ST
//Stop the EtherCAT network
ON StopMotionEngine DO
MLMotionStop();
END_DO;
FBD
FFLD
[Top]