MLPmpReadFstSpd
Descriptions
Get the FirstTravelSpeed parameter of a PMP block. This parameter is used as the first of 2 speeds in an MLPmpRel Motion Block. It is also used as the speed in an MLPmpAbs Motion Block.
Arguments
Input
| BlockID | Description | ID Name of a PMP function block in the Pipe Network |
| Data type | DINT | |
| Range | [-2147483648, 2147483648] | |
| Unit | N/A | |
| Default | — |
Output
| FirstTravelSpeed | Description | Present first travel velocity of the PMP PipeNetork Function |
| Data type | LREAL | |
| Unit | User unit/sec | |
| Default | Value defined in the setup of a PMP Block within a Pipe Network. It is in the “FIRST_TRAVEL_SPEED” field in the parameter tab |
Related Functions
Example
Structured Text
|
FirstSpeedValue := MLPmpReadFstSpd( PipeNetwork.PmpMaster ) ;
|
Ladder Diagram
Function Block Diagram
[Top]